Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE
Hi,
I am wondering what the timeout of the MCAN ROM bootloader is? Tech notes seem to indicate the RAM Bootloader is based off the ROM bootloader, the RAM bootloader states a timeout of first message to be 2 seconds, and timeout of consequent messages to be 11ms (commented in the code).
During testing I have sent data at 4ms interval, and the bootloading process fails. I have also tested using the SEND_TEST mode (which I believe to have an unlimited timeout and sends two test messages) and I can use this reliably.
I have modified the RAM application code (non SEND_TEST mode) to drive an output HIGH before the readMsg function and LOW after (after it times out). I seemed to measure slightly less than the specified 2 seconds, and significantly less than the stated 11ms, I measured approximately 2ms. I believe i can meet the first message timeout criteria but struggle to meet the lower consequent message timeout.
Can you please confirm:-
- The timeout of the first and consequent messages on the F28P65x?
- Is a 100ms delay needed between each message as stated in SPRUJH3 (Page41) - Getting Started with Bootloading on C2000 Microcontrollers? 100ms timeout does not seem to be included in the Host PC Peak example
- The only difference between SEND_TEST and normal mode is the removal of the timeout and it sends two test messages
Thanks in advance,
Andrew