Part Number: LAUNCHXL-F280039C
Other Parts Discussed in Thread: C2000WARE
No matter what I do, even though the Test Connection works prefectly, when i try to flash the device, i get:
IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.5.0.3902)
I've tried everything, SW3 set to 0,1, 1,0... any combo never works. Is it a known issue on Mac? I see that TI is very much Windows oriented and that leads me to think it may be the problem.
Is there anyone out there that has seen this issue and fixed it?
p.s. I've gone through this with Claude AI ad-nauseum, there must be a solution!