Hi,
I'm trying to run the IPC F28M35x MessageQ example with not too much success, I'm using CCSv5.1 IPC 1,24.0.16, XDC 3.22.4.46 and SYS/BIOS 6.32.5.54, I defined two projects one for the M3 and one for the C28 than I connected to the F28M35xx controlCARD to both M3 and C28, when I downloaded the code to the C28 or the M3 it starts flashing the code and than it never halts, is this the correct way to run the example? is there a need to change any switches on the board? SW7 is set to all 1 - Boot from M3 flash,
Many thanks,
HR