Part Number: F29H850TU

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: F29H850TU

Hi Ben,
Our datasheets are directly automated from the device spec so this is not a typo, though I will double check our other documentation to confirm. Likely this is a limitation of the pinmux for the smaller device packages
Regards,
Peter
Hi Ben,
I've reviewed our other documentation and specs and the pin mapping detailed in the datasheet is accurate. To give a little background, the EMIF mapping is taken from our F28P65x family of devices where this was not an issue since GPIO82 is available on the 176 pin package. However, on F29H85x, GPIO82 is only present on 256 BGA hence there will be this pinmuxing issue when trying to utilize both D2 and D27.
I will confirm with our design team on maximum intended bus width for this package but on my own review, I see there is also a limitation with D16 and D22 (due to other EMIF pinmux pins). This points to a maximum bus width of only 16-bit on these packages (at least for my review of the 176-pin package). And 32-bit on 256BGA. I recall a similar limitation on F2837x with smaller pin packages as well
Regards,
Peter