Part Number: C2000WARE
Category: C2000 Microcontrollers / Tools & Software
Environment
- OS: Ubuntu 25.10 (x86_64), VirtualBox
- Installer: C2000Ware_5_02_00_00_setup.run
- Installer type: BitRock InstallBuilder, 32-bit ELF binary
- Tested as: root user (login shell) and non-root user (sudo, and without sudo) — same result both ways
Problem
The C2000Ware 5.02.00.00 Linux installer fails immediately on launch with the following output:
Unable to initialize installer.
Is /tmp writable?
Is SELinux enabled? You may need to disable it temporarily.
SELinux is not enabled on this system. /tmp is writable and executable. These messages are red herrings.
(This is after including libc 32-bit libraries as required for the installer.)
Root cause identified via strace
I traced the installer at the syscall level. The failure sequence is:
- The installer correctly writes libtbcload1.7.so (a 2003-era Tcl binary extension, GCC 3.2.2) to /root/.installbuilder/tmp/libtbcload1.7.so.
- It then attempts to open the file using a literal tilde path: openat(AT_FDCWD, "~/.installbuilder/tmp/libtbcload1.7.so") — this returns ENOENT because the Linux kernel does not expand tilde characters. Tilde expansion is a shell feature only.
- The installer deletes the .so and exits with code 1.
Because this crash occurs before the Tcl runtime initializes, every command-line flag is silently ignored — including --mode unattended, --mode text, --help, and --debugtrace. There is no way to work around the failure using installer flags.
I also observed (unconfirmed) that libtbcload1.7.so may depend on Tcl symbols expected to be provided by the host process at dlopen time. Modern 64-bit Linux distributions do not carry a compatible 32-bit Tcl runtime, which may represent a secondary failure point even if the path issue above were resolved.
What was tried
- Running as root in a login shell
- Pre-creating /root/.installbuilder/tmp/
- Setting HOME explicitly on the command line
- All installer command-line flags (--mode unattended, --help, --debugtrace)
Potential avenues, if TI is able to share guidance
- Whether a filesystem workaround for the tilde path resolution is supported or advisable?
- Whether installing a specific 32-bit Tcl version and using LD_PRELOAD is a known fix?
- Whether a supported Linux distribution or kernel version exists where this installer works correctly?
Request
Please advise on a supported path to install C2000Ware 5.02 on Linux. Given that the installer bootstrap fails before argument parsing, further debugging on my end is limited without access to the installer source. A patched installer or an alternative distribution format (zip/tarball) would resolve this immediately.