This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: Help to choose the right µController

Part Number: TMS320F28P650DK

Hello, 

I am currently choosing a µC decdicated to develop motor drive applications and I hesitate between two series of µC :

  • C2000 with the current F28P650DK (and when it will be available maybe switch to the F29H85x familly)
  • Siatara with the AM263x familly

Here principal features that we aim to : 

  • Motor control: FOC (Field Oriented Control) at 200 kHz PWM (period 5 µs).
  • Position feedback : BiSS‑Cx2 for absolute encoder.
  • Communication bus : EtherCAT with FSoE for safety.
  • Safety function: Hold the motor in a safe position. We want this function to be certifiable up to IEC 61508 SIL 3.
  • I/Os : Standard motor drive interfaces: 6 PWM outputs, 3 current sense ADCs, SPI for encoder, GPIOs, ABN for Hall sensors and incremental encoders, DC bus voltage measurement etc..

If there is better choice of µC who came in mind, I am also interested.

Best regards,

Yanis Maacha