Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H85X-SDK: SDL dependencies onto the SDK

Part Number: F29H85X-SDK

Hello,

Is the F29 SDK actually independent from the F29 SDK? The concern here is that the SDL will be safety qualified when the SDK will not, so if the SDL depends on the SDK, this would break the safety qualification.

For example, I see in the ADC example sdl_adc_os_detect_example.c calls to ADC_setINLTrim(), which is an SDK function. So it looks like customers have to provide their own SDL support functions similar to the SDK functions... Am I missing anything?


Best regards,
François.

  • Hi Francois,

    Let me check with F29 SDK team and get back to you.

    Thanks,

    Ira

  • The SDL library itself doesn't call any SDK functions, so in that sense it's independent.  You are right that users are responsible for some configurations before running the SDL functions though--configuring SYSCLK, GPIOs, ADC trims, Interrupts, etc... In our examples, we use the driverlib functions which aren't FSQ, so customers will either have to qualify those for safety themselves or use an MCAL equivalent (since MCAL will be FSQ).