Part Number: C2000WARE-DIGITALPOWER-SDK
Other Parts Discussed in Thread: TMS320F280049C, PMP23126, C2000WARE

You can post the following on the TI E2E C2000 forum:
Hi TI Experts,
I am working on a Phase Shifted Full Bridge (PSFB) DC-DC converter using the TMS320F280049C controlCARD / LaunchPad for PWM generation.
For reference, I am following the TI application report:
PSFB Control Using C2000 Microcontrollers (SPRABR1)
In my design, synchronous rectification MOSFETs are used on the transformer secondary side (similar to Q5 and Q6 shown in the application report). I am using MATLAB/Simulink with the C2000 Microcontroller Blockset for PWM generation and code generation.

Currently, I am facing difficulties generating the synchronous PWM signals for the secondary-side MOSFETs. The primary-side phase-shifted PWM generation is working, but I need guidance on implementing the SR PWM logic correctly in Simulink for the F280049C.
My questions are:
-
What is the recommended method to generate synchronous rectifier PWM signals for PSFB on F280049C?
-
Should separate ePWM modules be used for SR MOSFETs with synchronization through TBPHS/Sync chain and dead time control for the generated PWM?
-
Is there any TI example project, reference code, or Simulink model available for secondary-side SR PWM generation in PSFB topology?
-
Can this be implemented efficiently using ePWM synchronization only, or is CLB also recommended?
-
Are there any specific considerations while implementing this using the C2000 Simulink Blockset?
I also checked the following TI references:
Any guidance, waveform generation approach, or example configuration would be very helpful.
Thanks,
Mayank Kumar