Part Number: C2000WARE
Other Parts Discussed in Thread: TMS320F280025C
Problem: When customers use the 28002x product, they encounter program runaway issues. Using our company's host computer software, it was confirmed that only the bootloader (a private bootloader written after address 0x80000) exists in the chip. Rewriting the APP portion with the private bootloader allows it to work normally again. Currently, it is unclear whether the issue lies with the private bootloader, the APP portion, or the chip itself.
Now, there is a faulty device. I want to only connect to the board via emulation (debug probe) to inspect which part of the code in the flash is problematic. Previously, I tried following configuration tutorials, but each time I connected via emulation, either the flash got erased, or if connected without erasing, I couldn't view the data in the flash. Do you have standard operating instructions for this? P.S. The project has DCSM passwords configured, but normal emulation erase/write operations can successfully program the chip, so this should not be a hindrance.