This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280037C: Flash Programming

Part Number: TMS320F280037C
Other Parts Discussed in Thread: TMDSEMU200-U, TMS320F280039C

I've designed a circuit according to datasheet for programming of microcontroller which is tms320f280037c and with that circuit i'm able to do program in RAM of microcontroller with XDS200 Debug Probe (TMDSEMU200-U) but not able to do program in Flash.
i've connected all VDDIO pin of microcontroller to 3.3V and all VSS pin to GND.
so i want a solution for programming in flash. is there any proper circuit available for f280037c where i can program in both ram and flash.Screenshot 2026-05-14 175545.png