This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Boot problem with dual core usage with custom code

Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE

Hello,

I am trying to program both CPU1 and 2 of 28379D IC mounted on a  customized design board through MATLAB auto code generator. I am able to flash the CPUs through external XDS110 debugger.  However,  after flashing its not possible to run the program as it has certain boot mode issue. One work around I found out was to follow this exact sequence--- 1. flash CPU2 code in to CPU2 2. flash blinky in to CPU1 (LED blink example code provided in controlSUITE to run in flash mode) 3. flash CPU1 code in to CPU1. However the same needs to be repeated with every power cycle.

As this is very inconvenient, I am looking for a solution to this problem. 

current version of CCS---20.3

current version of MATLAB---2026A

GPIO 72 and 84--high

(we have tried the same with CCS 12.7, MATLAB 2024B, and a similar board which has worked before which rules out hardawre oroblem)

Please help to resolve this.

Thanks,

Jayanti