This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H85X-SOM-EVM: Information regarding HSM services.

Part Number: F29H85X-SOM-EVM

Hi,

Currently, HSMrt includes HSM services; however, these services do not provide crypto accelerators such as AES, SHA, and PKA, which are required for secure communication and data validation in communication networks during runtime.

Are there any plans to provide support for these crypto accelerator services in future releases?

Regards,

Shashank

  • Hi Shashank,

    The latest TIFS(v26.00.00) includes MAC services which basically send a request from C29 side over SIPC to HSM, then HSM computes the HMAC/CMAC/GMAC and sends it back to C29.
    TIFS also contains all the required Crypto drivers, with RTDMA enabled now in the latest release.
    The MAC Services can also be used as a reference by the customer to extend support for other crypto algorithms.

    Thanks and Regards,
    Aditya Singal