Part Number: LAUNCHXL-F28P65X
I am trying to generate MHz(nearly 5 MHz) range PWM for a (open-loop currently) phase shift full bridge converter or a push pull converter to build a RF power supply. Need more control over the phase-shift hence, need high resolution PWM. Can LAUNCHXL-F28P65X provide and help with the same as it has a HRPWM module too. Need to know if this DSP would work or need some recommendations for a DSP which would be able to facilitate the requirement metioned above.