Hi There
(F28027PT piccolo ControlSTICK)
I am getting confused with the A/B designations used for the names of SOCs/ ADC channels and ePWM Triggers.
I have set SOC0 to ADC A1, SOC1 to ADC B1 and SOC2 to ADC B2.
They are all set to be triggered by ADCTRIG9 (ePWM3, ADCSOCA)
However I wish the trigger to be taken from ePWM3B, is the 'B' here linked to the 'B' of the above ADCTRIG ADCSOC ?
Should I be using ADCSOCB for ePWM3B? or for ADC B1 and ADC B2 and ADCSOCA for ADC A1?
Thanks