This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SYSCONFIG: Clarification on SysConfig vs Driverlib/Register-Based Development in C2000 Projects

Part Number: SYSCONFIG
Other Parts Discussed in Thread: C2000WARE,

Hi,
I’m currently working on driver development for C2000 MCUs (F28P55x family), and I have a clarification regarding the preferred development approach.

In our workflow, we see multiple ways to configure peripherals such as SPI, Timer, ADC, PWM and Watchdog:

  1. Using SysConfig-generated code (board.c/.h)
  2. Using C2000Ware driverlib APIs directly (manual configuration)
  3. Referring to TI example projects
  4. Using direct register-level programming

    I would like to understand the recommended industry approach for production-level firmware development:
  • Is SysConfig-based development preferred for embedded projects, and if so, why?
  • What are the specific advantages of SysConfig beyond ease of configuration (e.g., pinmux consistency, clock configuration safety, error checking, optimization)?
  • Does SysConfig have any impact on code optimization or runtime efficiency, or is it mainly a configuration and development productivity tool?
  • In which scenarios would developers avoid SysConfig and instead use:
    • only driverlib APIs, or
    • direct register-level programming?
  • How should we balance between:
    • SysConfig-generated initialization code
    • custom HAL/BSW written by developers
  • For long-term maintainability and scalability (large projects with multiple peripherals), what approach is commonly followed?

Understanding this will help us define a consistent methodology for BSW design across modules.

Thanks in advance for your guidance.

  • Hi Vishwa,

    SysConfig is TI's recommended starting point for peripheral configuration on C2000 MCUs, and the recommended production architecture layers SysConfig-generated initialization with C2000Ware driverlib APIs for runtime control.

    Sys Config is TI's recommended starting point for all your projects. SysConfig is a graphical utility that "helps you manage, expose and resolve conflicts visually" and outputs "C header and code files that can be used with SDK examples or used to configure custom software". TI's own F28P55x examples use this approach — the SPI loopback example explicitly states that "the pinmux and SPI modules are configured through the sysconfig file".

    2. Specific Advantages of SysConfig

    Advantage
    Detail
    Pinmux conflict resolution
    Automatically selects valid pin assignments and visually exposes conflicts 
    Cross-device portability
    Migration across C2000 families by simply updating the .syscfg board specification 
    Configuration consistency
    Generates deterministic initialization code from a single source of truth
    Error prevention
    Catches invalid combinations at configuration time rather than runtime
    Clock/peripheral integration
    Enhanced clocktree integration for communications peripherals 

    3. Impact on Code Optimization / Runtime Efficiency

    SysConfig is primarily a development-time configuration and code-generation tool, not a runtime optimization tool. The generated code calls the same driverlib APIs you would call manually. There is no evidence of runtime overhead beyond what equivalent hand-written driverlib calls would produce.

    4. When to Avoid SysConfig

    Scenario
    Preferred Approach
    Timing-critical ISR paths where every cycle counts
    Direct register access
    Legacy codebase integration with existing register-level drivers
    Driverlib or register-level
    Peripheral behavior not yet supported by SysConfig modules
    Driverlib APIs directly
    Ultra-fine-grained runtime reconfiguration (e.g., dynamic SPI mode switching mid-operation)
    Driverlib APIs
    Driverlib abstraction overhead unacceptable (rare, but possible in tight control loops)
    Direct register writes

    The driverlib functions map directly to hardware registers, so the abstraction cost is minimal in most cases. Direct register programming should be the exception, not the rule.

    5. Balancing SysConfig + Custom HAL/BSW

    The recommended architecture for production F28P55x projects:

    ┌─────────────────────────────────────┐
    │ Application Layer │
    ├─────────────────────────────────────┤
    │ Custom HAL / BSW │ ← Your team's abstraction
    │ (runtime control, state machines, │
    │ error handling, mode management) │
    ├─────────────────────────────────────┤
    │ C2000Ware Driverlib APIs │ ← Runtime peripheral control
    ├─────────────────────────────────────┤
    │ SysConfig-generated board.c/.h │ ← One-time initialization
    ├─────────────────────────────────────┤
    │ Hardware (F28P55x) │
    └─────────────────────────────────────┘
    SysConfig owns: Pin assignment, peripheral clock enables, initial register configuration, GPIO mux
    • Your BSW/HAL owns: Runtime logic, interrupt handlers, state management, error recovery, dynamic reconfiguration
    • Driverlib: The API layer both SysConfig and your BSW call into

    This separation keeps SysConfig's strengths (conflict-free initialization, portability) while preserving full control where your application logic demands it.

    6. Long-Term Maintainability for Large Projects

    For multi-peripheral projects, the combination above is the most sustainable because:

    • SysConfig centralizes hardware mapping — when pin assignments change or you migrate to a new board variant, you update one .syscfg file rather than hunting through scattered init code
    • Driverlib provides device abstraction — C2000Ware is designed to "minimize development time" with "device-specific drivers, libraries, and peripheral examples"
    • Custom BSW remains hardware-agnostic — your application logic doesn't embed pin numbers or register addresses
    • Functional safety support — TI provides the Software Diagnostic Library (SDL) as part of C2000Ware for safety-critical applications (ASIL B/SIL 2 certified hardware), which integrates with this layered approach

    Thanks,

    Ira

  • Thanks for the detailed clarification.