Part Number: TMS320F280025
Hi
We use the F280025 in our solar inverter project ,and now, we have below issue for the ADC:
- Our ADC initial configuration:

The initial pin configuration:

Our issue is: a. The power is less than 2KW, read the register of A1=1550, it is consistent with input;
b. The power is more than 2KW, the voltage of the A1=1.2V, and read the register of A1=59
c. We change the adccRegs. ADCSOC0CTL. bit. ACQPS to 18, the A1 is normal, But as the power
increases, the ADC result registers of A0=2000 and A8=1200;
2. We Change the channel of the ADC will cause interference and actual inconsistency in the sampling of
other channels:
a. A9 sampling decreases as the power increases. At the same time, the sampling results of the two channels
of A1 are also different;

b. We change the below ADC configuration and the A9 and A0 sampling is normal:

c. Please advise that why this ADC need to set as above?
3. We change the adccRegs. ADCSOC0CTL. bit. ACQPS from 18 to 30, the result is also abnormal;
4. Plesae kindly check the below schematic diagram and our ADC configuration, and provide your comment that
how to solve this issue, thanks.