Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: TIDA-010992, , C2000WARE-MOTORCONTROL-SDK
Hi experts,
TIDA-010992 is the reference design that seems to be the closest to the application currently being considered by our customer.
Note: If I create a thread with the device set to “TIDA-010992,” the thread is created in the Arm based microcontroller forum. Therefore, I am creating this thread with the device set to “TMS320F28P650DK.”
It does not seem to be included in C2000WARE-MOTORCONTROL-SDK v6.0.0.0.
Q2: Is there any software flowchart or similar documentation available?
Q3: Is there any information available about the motors and encoders used in this reference design?
Since this is a humanoid robot hand reference design, I would like to understand which part of the finger or hand each motor is intended to control.
Q4: What is the purpose of connecting an external CPU via EtherCAT?
This reference design appears to be configured with a single TMS320F28P650DK. I would like to understand whether the commands to each motor are assumed to be handled entirely within this reference design, or whether an additional device such as an AM26x or AM24x is required.
Best regards,
O.H