This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD280039C: Pin mismatch between control card and HSEC8 connector

Part Number: TMDSCNCD280039C
Other Parts Discussed in Thread: C2000WARE

Hi,

This is Karthik from SnapMagic.

One of our users reported a pin mismatch between the TMDSCNCD280039C control card and the HSEC8 connector (Part Name: HSEC8-160-01-L-DV-A-BL)

The user noted that the control card has an insertion slot between pins 55 and 57, whereas the connector footprint has the insertion gap between pins 63 and 65. Additionally, the user noted that the pin numbering sequence appears reversed between the control card and the connector footprint. 

   

image.png

Based on the connector datasheet, we have verified that the footprint's insertion gap location and pad numbering sequence match the manufacturer's specifications. However, the user is experiencing difficulty inserting the control card into the HSEC connector.

Could you please clarify whether the user is using the correct connector for the TMDSCNCD280039C module, or if there are any additional requirements or considerations for properly mounting the module to the connector?

Thank you for your assistance.

Best Regards,

Karthik

hsec8-1xxx-xx-xx-dv-x-xx-footprint.pdf hsec8-1xxx-xx-xx-dv-x-xx-x-xx-mkt.pdf