Part Number: TMS320F280049C
Hi,
I use TMS320F280049C to configurate ADC-A: SOC0, SOC1,SOC2,SOC3 to sample different analog signals. And set up SOC1 for ADC interrupt trigger source.
And in related ADC ISR(triggered by SOC1) to collect all data(include SOC2 and SOC3), my question is: is there any issue about this method? I know when at the time read SOC2 and SOC3 ADC result register, the SOC2 and SOC3 maybe have not complete ADC conversion, so what's the value in SOC2 and SOC3 result register? the value is zero? or it will keep the previous value(if previous have value not zero)?
Another question is how much time will it take for write the ADC value to ADC result register when finish ADC conversion? Is there any possible when CPU read the ADC result register conflict with writing to result register?