Part Number: TMS320F280039C-Q1
Hi all,
2. Could external pin voltage levels, ambient temperature, or the operating condition of the CAN transceiver affect the Busy bit staying continuously set to 1? My understanding is that the Busy bit in CAN_IF1CMD and CAN_IF2CMD registers reflects an internal MCU data transfer status and is unrelated to external peripherals — is this correct?
3. Under what operating conditions would the Timer module's overflow flag fail to be set to 1? (The MCU crystal oscillator has been verified as normal, and PWM output is also normal.)