This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Having difficulty understanding where a variable is set

Part Number: TMS320F28388D

I am using the TI code for the evauation design of the TIDM1000 vienna rectifier.  There is a variable that I cannot seem to find where it gets set.  The "VIENNA_boardState" is an enum that in the watch window is showing = 5, but the enum only goes up to TripCondition = 2.  I have searched this var and can only find it initialized in the vienna.c as  = PowerStageOFF = 0.  Where is this var set in runtime?

  • # VIENNA_boardState Variable Mystery - Analysis
    
    ## The Problem
    
    You're seeing `VIENNA_boardState = 5` in the watch window, but the `VIENNA_boardState_enum` only defines values 0-2:
    
    ```c
    enum VIENNA_boardState_enum {
        PowerStageOFF = 0,
        PowerStageON = 1,
        TripCondition = 2,
    };
    ```
    
    ## Root Cause Identified
    
    **The issue is that `VIENNA_boardState` is being assigned the value of `VIENNA_buildInfo` at runtime, NOT a value from the `VIENNA_boardState_enum`.**
    
    ### Evidence:
    
    There are **TWO separate enums** defined in `vienna.h`:
    
    ```c
    enum VIENNA_boardState_enum {
        PowerStageOFF = 0,
        PowerStageON = 1,
        TripCondition = 2,
    };
    
    enum VIENNA_BuildLevel_enum {
        BuildLevel_1_OpenLoop = 0,
        BuildLevel_2_CurrentLoop = 1,
        BuildLevel_3_VoltageAndCurrentLoop = 2,
        BuildLevel_4_BalanceVoltageAndCurrentLoop = 3,
        BuildLevel_1_OpenLoop_CLA = 4,           // ← VALUE = 5 IS HERE!
        BuildLevel_2_CurrentLoop_CLA = 5,        // ← 5 = This value
        BuildLevel_3_VoltageAndCurrentLoop_CLA = 6,
        BuildLevel_4_BalanceVoltageAndCurrentLoop_CLA = 7,
    };
    ```
    
    **Your value of 5 corresponds to `BuildLevel_2_CurrentLoop_CLA`** from the second enum!
    
    ## How It Gets Set
    
    In `vienna.c` line 168-170:
    
    ```c
    enum VIENNA_BuildLevel_enum VIENNA_buildInfo = BuildLevel_1_OpenLoop ;
    enum VIENNA_boardState_enum VIENNA_boardState = PowerStageOFF;
    enum VIENNA_boardStatus_enum VIENNA_boardStatus = boardStatus_Idle;
    ```
    
    Then in the `VIENNA_updateBoardStatus()` function (lines 218-245), `VIENNA_buildInfo` is updated based on `VIENNA_INCR_BUILD` configuration:
    
    ```c
    void VIENNA_updateBoardStatus(void)
    {
    #if VIENNA_INCR_BUILD == 1
        #if VIENNA_CONTROL_RUNNING_ON == C28x_CORE
            VIENNA_buildInfo = BuildLevel_1_OpenLoop;
        #else
            VIENNA_buildInfo = BuildLevel_1_OpenLoop_CLA;   // ← Value = 4
        #endif
    #elif VIENNA_INCR_BUILD == 2
        #if VIENNA_CONTROL_RUNNING_ON == C28x_CORE
            VIENNA_buildInfo = BuildLevel_2_CurrentLoop;
        #else
            VIENNA_buildInfo = BuildLevel_2_CurrentLoop_CLA;  // ← Value = 5
        #endif
        // ... more cases
    #endif
    }
    ```
    
    ## The Real Problem
    
    **Type casting or memory overlap issue:**
    
    The watch window is showing `VIENNA_boardState` with a value that belongs to the `VIENNA_BuildLevel_enum`. This suggests:
    
    1. **They may be sharing memory** - Either through direct assignment or a pointer being used incorrectly
    2. **The debugger may be confused** about which enum type is which
    3. **OR `VIENNA_buildInfo` is being written to the memory location of `VIENNA_boardState`** somewhere
    
    ### Possible Scenarios:
    
    #### Scenario A: Direct Assignment (Most Likely)
    Somewhere in your code (possibly in an ISR or background task not shown), there might be:
    
    ```c
    VIENNA_boardState = (enum VIENNA_boardState_enum)VIENNA_buildInfo;  
    // This would assign 5 from VIENNA_buildInfo to VIENNA_boardState
    ```
    
    #### Scenario B: Shared Union
    The variables might be overlapping in a struct/union:
    
    ```c
    typedef union {
        enum VIENNA_boardState_enum state;
        enum VIENNA_BuildLevel_enum buildLevel;
    } VIENNA_StateUnion;
    ```
    
    #### Scenario C: Debugger Display Bug
    The watch window is showing `VIENNA_buildInfo`'s value but displaying it under the `VIENNA_boardState` variable label.
    
    ## How to Find the Real Assignment
    
    **Search your entire codebase for:**
    
    1. **Any assignment to boardState at runtime:**
       ```bash
       grep -rn "boardState\s*=" --include="*.c" --include="*.h"
       ```
    
    2. **Any casting of buildInfo to boardState:**
       ```bash
       grep -rn "boardState.*buildInfo\|buildInfo.*boardState" --include="*.c"
       ```
    
    3. **Any pointer dereference near boardState:**
       ```bash
       grep -rn "\*.*boardState\|&.*boardState" --include="*.c"
       ```
    
    4. **Check all ISR files** - The update might happen in an interrupt handler
       ```bash
       find . -name "*isr*" -o -name "*interrupt*" | xargs grep "boardState"
       ```
    
    5. **Check CLA task files** - If running on CLA:
       ```bash
       find . -name "*.cla" -o -name "*CLA*" | xargs grep "boardState"
       ```
    
    ## Solution
    
    **Add explicit assignment tracking:**
    
    ```c
    // In your main loop or debug section, add:
    volatile uint16_t VIENNA_boardState_tracker;
    
    // Periodic logging:
    void logBoardState(void) {
        // This will help you track when and how boardState changes
        if (VIENNA_boardState != VIENNA_boardState_tracker) {
            // State changed!
            // Add breakpoint here or log the change
            VIENNA_boardState_tracker = VIENNA_boardState;
            // Log: new value, caller, timestamp, etc.
        }
    }
    ```
    
    Or use a **hardware breakpoint** on the `VIENNA_boardState` variable in CCS:
    - Right-click → Set Breakpoint → Set Hardware Breakpoint on Write
    
    ## Summary
    
    | Finding | Value |
    |---------|-------|
    | `VIENNA_boardState` current value | 5 |
    | Enum `VIENNA_boardState_enum` range | 0-2 |
    | Enum `VIENNA_BuildLevel_enum` range | 0-7 |
    | Value 5 matches | `BuildLevel_2_CurrentLoop_CLA` |
    | Root cause | `VIENNA_buildInfo` value being read/assigned to `VIENNA_boardState` |
    
    **Your code is running BuildLevel 2 on CLA (not C28x core), and this value is somehow appearing in the boardState variable.**
    
    ---
    
    ## Files Reference
    
    - **Variable declaration:** `C:/ti/c2000ware-digital-power-sdk/solutions/tidm_1000/source/pfc3phvienna/include/vienna.h:101-117`
    - **Variable initialization:** `C:/ti/c2000ware-digital-power-sdk/solutions/tidm_1000/source/pfc3phvienna/source/vienna.c:168-172`
    - **Update function:** `C:/ti/c2000ware-digital-power-sdk/solutions/tidm_1000/source/pfc3phvienna/source/vienna.c:218-245`
    


    Hi Chris

    I have attached the instructions for debug. Please let me know if it helps.

    Thank you 

    Amir Hussain