Part Number: TMS320F28388D
I tried to set up the McBSP to have both TX and RX use the same pin for FS and CLK which are MFSX and MCLKX.
It doesn't seem to me that RX side can be triggered using MFSX and MCLKX. I setup the config to work around that by using sample rate generator to generate TX and supply RX.
The problem I have is that the MFSX pin and MFSR pin are not synced. I see that the MFSX and MFSR are 700ns apart.
Here is my config: