Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: Random issues Debugging + Flashing

Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: UNIFLASH

Hello,

Up until fairly recently I have had no problems on a custom board with the P65x. A few weeks ago I began development on a SSBL and noticed that a bunch or issues arrose with debugging and flashing the controller after 4-6 months of no problems.

lash banks that the user would like the flash plugin to erase (in the CPU1 flash plugin GUI and the CPU2 flash plugin GUI)
C28xx_CPU1: Warning: Failed unlocking device (zone 1) after reset.
C28xx_CPU1: Warning: Failed unlocking device (zone 2) after reset.
C28xx_CPU1: Trouble Setting Breakpoint with the Action "Remain Halted" at 0x10058: (Error -1066 @ 0x10058) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 20.0.0.3283) 
C28xx_CPU1: Breakpoint Manager: Retrying with a AET breakpoint
C28xx_CPU1: GSxMSEL register configured correctly
C28xx_CPU1: BankMuxSel register configured correctly
C28xx_CPU1: Trouble Setting Breakpoint with the Action "Remain Halted" at 0x1010c: (Error -1066 @ 0x1010C) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 20.0.0.3283) 
C28xx_CPU1: Breakpoint Manager: Retrying with a AET breakpoint
C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0)
C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash.  If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: Breakpoint Manager: Retrying with a AET breakpoint

After doing some research, it looks like the device cannot unlock specific zones in flash to program but I have never worked with the DCSM? It seems the only way to fix this is to perform a bunch of memory operations via Uniflash (don't know why this works is it a different GEL file maybe?) like erasing all of flash and reflashing several times and if I am lucky it will recover. I also noticed that most of the scripts on Uniflash require me to manually reset the controller with our push button or else they hang on OnTargetConnect().

I tried to revert all my changes from _cint00 and the linker cmd file back to what they were and now none of my projects can load or flash.

Any suggestions on how to proceed with debugging if / how the device was locked would be great. I followed the instructions in a similar forum with no success.

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1066378/tms320f280049-trouble-setting-breakpoint-with-the-action-remain-halted-at-0xc0d4

 

  • EDIT: Just FYI I have been doing some further diagnosis, I am able to attach to a live session on a flashed device (after flashing through Uniflash) by right clicking the CCXML for the project and starting a "Project-Less Debug" and manually loading the ELF file. My program seems to be running fine. Just wondering if the GEL file for Uniflash differs from the one loaded in CCS. Thanks

  • Hello,

    The GEL files should be identical between CCS and UniFlash. What version of UniFlash are you using? Does the issue occur when the device is configured for WAIT boot?

    Best,
    Matt