TMS320F28P550SJ: F28P55 USB Flash Kernel

Part Number: TMS320F28P550SJ
Other Parts Discussed in Thread: C2000WARE

Hi, 

I'm trying to USB Boot mode for TMS320F28P55;

I successfully completed the connection with use "usb_flash_programmer.exe -l" and downloaded an example project.

The question is: is there a USB Flash kernel similar to the one in device_support\f2837xd\examples\dual\F2837xD_usb_flash_kernels for F28P55?

Thanks!

 

  • Hi, 

    There is no USB flash kernel example, but you can refer the SCI Flash kernel example available in 

    <C2000Ware>\driverlib\f28p55x\examples\flash folder

    Alternative is to port the existing USB Flash kernel for F2837xD to F28P55x.

    Best Regards

    Siddharth