Other Parts Discussed in Thread: CONTROLSUITE
Hi folks, some newbie help needed. I just purchased the concerto controlcard and dock (TMDXDOCKH52C1) and I'm having trouble speaking to it from CCS and running the basic (blinky_c28) project.
- I have installed CCS v4 that comes on the CD (version 4.2.4.0003 - code composer studio core edition)
- I went into controlSuite and installed the support files (ti_c2000support_setup 2.0.0.14.exe)
I can successfully build the blinky project (the one in the controlSuite\device_support\f28m35x\v110\...\blinky
Next, do I plug in the USB cable from the Docking board to my laptop, or from the controlCard? I have tried it both ways and I get a TI XDS100v1 in the one case (when plugged to the docking board) and TI XDS100v2 in the other case. Do I leave them both plugged in?
When I create a new Target Configuration, and use the XDS100v2 USB emulator, there is no device/board that matches the concerto (what should I see?)?
What now? Somewhat anxious to start playing with my new toy!
Thanks for your help
SA