This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H859TU-Q1: RAM initialization during startup

Part Number: F29H859TU-Q1

Hello,

I found in the TRM that the bootrom clears all the RAMs only on a power on reset.

But are there other players (HSM for example) that could initialize or write into the RAMs other than the M0 RAM during startup in Flash boot mode ?

If yes,

  • Which RAMs / address ranges are impacted ? On which resets ?
  • Where can I find this information ?

Thank you