This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P550SJ: File name too long error when installing tiny-tensorlab

Part Number: TMS320F28P550SJ

Hi Experts,

I have below errors install the tiny-tensorlab, could you please help looking into it?

image.png

Regards,

Hang

  • Mentioned in the User Guide: Link

    Windows users must enable long path support before cloning.

    Windows has a 260-character path limit by default, which can cause issues with the deeply nested directory structure in tinyml-* repositories. Run this command before cloning:

    git config --global core.longpaths true
    

    This allows Git to handle paths longer than 260 characters globally. You only need to run this once per system.

    (Run the above git command & then proceed to cloning/installation)