Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE, CODECOMPOSER
CCS Version: Version: 21.0.0.14__1.12.0; Default VS Code API: 1.110.1
C2000Ware Version : 26.01.00.00.STS
Everything is installed to the default location C:\ti\
I want to open an example project. Thus, I select the following example project:
[HOME symbol] / C2000 real-time controllers / Embedded Software / C2000Ware / English / Libraries / Communications / Ethercat / Examples / F28P65X / Ethercat CPU1 PDI HAL TEST CCS Project
I start by hitting the "Import" button. CCS installs two libraries (both 'successful'), then when hitting the 'confirm' button:

This happens again and again. It does not matter if there is a folder open in the explorer panel or not.
What is going wrong?