Part Number: TMS320F280025C
Custom board with a msp430 controlling the bus. Targets include a f280025c and other devices. Cold boot and everything works fine. After flashing the f280025c bus locks up with both SCL and SDA pulled low. If a debugging session is started, SCL get pulled low until the MSP addresses a different device (expected, since the f280025c's address is NACKed (and clock stretched?)). Starting the debugger both SCL and SDA stay low.
Of note, the f280025c is using the internal oscillator and GPIO18_X2 and GPIO19_X1 used for i2c.
Tried toggling the configuration of the GPIO's as open drain, but doesn't seem to help. I there anything else that might clear this up?