Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H85X-SDK: F29H85X DCL Documentation

Part Number: F29H85X-SDK
Other Parts Discussed in Thread: SYSCONFIG

Hello,

we are currently trying to integrate the DCL into an F29H85x project using SysConfig. Unfortunately, it appears that only a single instance of a controller can be configured, whereas our use case requires multiple controllers with different parameter sets.

Is it correct that only one controller instance is supported in this setup?

Additionally, is there any documentation available describing the DCL implementation for the F29 SDK? The materials we have found so far mainly refer to the C28x and CLA implementations. Even the “Detailed Description” in SysConfig seems to focus on the F28's CPU and CLA.

Best regards