Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000-SAFETI-DIAGNOSTICS-LIB, MIDAS, C2000WARE
Hi experts,
The customer is considering using the F28P650, and functional safety is required for their application.
Q1:For the SDL (C2000-SAFETI-DIAGNOSTICS-LIB), is there any plan to provide a certified SDL version for F28P65x with a Compliance Support Package (CSP)?
Q2:Would it be possible to provide the following documents?
- Device FMEDA: SafeTI tunable FMEDA / MIDAS FMEDA database
- Safety Analysis Report (SAR)
- Safety Report
- Safety Report Summary, including DFA and common-cause failure analysis
Q3:Could you please confirm whether the latest version of C2000 MISRA-C Policy (SPRACB3) is “SPRACB3 – September 2017”? Also, is there any policy or roadmap for MISRA C:2025 support and/or MISRA C++ support?
We would like to confirm whether the above information is available, and if there is any planned schedule for availability. Since the customer has already executed an NDA, if this information can be obtained by contacting the local sales team, it would be helpful if you could reply accordingly.
I will loop this thread.
Best regards,
O.H