This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800132: POR / BOR need confirmation

Part Number: TMS320F2800132

Dear support team,

I need a few confirmation about POR / BOR on TMS320F2800132.

In case of POR, a bit is set in RESC, this bit is cleared by boot ROM but we can have it using the boot ROM status. This is quite clear.

Now I would like to clarify what's happen in case of BOR, from the TRM:

"A BOR resets everything in the same manner as a POR reset."

Does it mean that it will set the same bit in RESC and boot ROM status than POR?

Regards