This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000WARE-DIGITALPOWER-SDK: USB CDC Support on F28377S LaunchPad

Part Number: C2000WARE-DIGITALPOWER-SDK
Other Parts Discussed in Thread: TMS320F28377S

Hi,

Can I connect the TMS320F28377S LaunchPad directly to a PC using the USB signals (D+, D−, and GND) through the LaunchPad headers on GPIO42 (USBDM) and GPIO43 (USBDP), and have the device enumerate as a USB CDC (Virtual COM Port) on the PC?

  • Hi,

    While the F28377S chip itself contains a USB peripheral, the LAUNCHXL-F28377S physical board lacks a dedicated USB data connector routed to the peripheral pins. 
    Hence, you will need to have blue wiring as you have mentioned. Pls ensure that the pins are mapped correctly (USB signals to the GPIO pins)

    Best Regards

    Siddharth