Hi,
I am at Level 4 of sensorless PMSM (DRV8312-C2-KIT_v127\PM_Sensorless) with a combination of F28069 exp kit and a custom power board. I am tuning the PID values with intial P=0.05;I=0.00005 and D=0/T. The code starts smoothly running the motor to 6 RPM (Speedref = 0.01). Motor keeps rotating. After some time the exp kit stops updating the graphs and hangs. I could not change the values real time as the kit is hanged.
Again I have to shut down the kit, restart and load the programm to the processor. Again the problem repeats. Is there any problem with exp.kit?. And how to sort it.
Thx & Rgds