Part Number: F29H85X-SOM-EVM
Other Parts Discussed in Thread: SYSCONFIG
Hello,
I installed Sysconfig standalone and tried to run it. When I try to debug and see in the event logs, i get the following:
Faulting application name: nw.exe, version: 0.94.0.0, time stamp: 0x665bfc50
Faulting module name: ntdll.dll, version: 10.0.26100.8521, time stamp: 0xccc028d4
Exception code: 0xc0000005
Fault offset: 0x0000000000164747
Faulting process id: 0xAF9C
Faulting application start time: 0x1DD10450525FB25
additionally,
when I check the task manager, the sysconfig instance opens but closes down within a few second on its own.