This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H85X-SOM-EVM: CLB tile usage

Part Number: F29H85X-SOM-EVM

Hello,

I want to implement a bi-directional approach. For specific reasons, I need CLB configuration for the switch signals. However the number of switch signals exceed the number of available CLB instances that can be setup. Another way that I want to explore is, if I can initialise multiple tile designs for a single CLB instance and switch between them based on the mode/condition I want the system to operate. Is this a possible way to implement or is it only possible to have 6 tile configurations, one for each instance?