This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F29H850TU: CLB input configuration issue

Part Number: F29H850TU
Other Parts Discussed in Thread: SYSCONFIG

Hi there, 

Im trying to use clb 5 and clb6 for an application. When I try to use global mux for input confuguration to select EPWM5 and EPWM6 is throws an error and doesn't allow me to set it up. Following are the logs that it shows:


Oh Snap! The last change caused an exception...

TypeError: Cannot read properties of undefined (reading 'displayName')

at Object.validate (C:\SRC\shared\ti-f29h85x-sdk-gh\5d25\source\driverlib\.meta\clb.js:695:41) at ee.validate (webpack://sysconfig/src/pinmux/services/objectManagers/moduleInstance.ts:640:16) at iteratee (webpack://sysconfig/src/pinmux/services/instanceContainers/module.ts:157:55) at tc (webpack://sysconfig/node_modules/lodash/lodash.js:530:11) at rh.each (webpack://sysconfig/node_modules/lodash/lodash.js:9409:59) at y.validate (webpack://sysconfig/src/pinmux/services/instanceContainers/module.ts:157:5) at iteratee (webpack://sysconfig/src/pinmux/services/metaEnvironment/runtimeContext.ts:341:6) at tc (webpack://sysconfig/node_modules/lodash/lodash.js:530:11) at rh.each (webpack://sysconfig/node_modules/lodash/lodash.js:9409:59) at W.validate (webpack://sysconfig/src/pinmux/services/metaEnvironment/runtimeContext.ts:340:5)



Also, could you please confirm if the two are the same? The image that shows EPWM5AE and EPWM6AE are from a different project and the image EPWM5A (CLB5-6) and EPWM6A (CLB5-6) correspond to another. However, I want to replicate the approach in the project where the inputs are listed as 'EPWM5A (CLB5-6) and EPWM6A (CLB5-6)' but I do not see them listed in options of the drop down list. 

 

 CLBS.png, the image which shows  CLBE.png