Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DH: Problem with isolated XDS110 debug probe

Part Number: TMS320F28P650DH

Hello,

I´m working with CCS12.6 and a the standard XDS110 emulator probe and I want to switch to the isolated XDS110 probe. The probe is correctly installed but after start of the debugger I got the following message:

 

image.png

 

What is the reason for this problem?

 

Thank you very much

 

Ralf

  • Hi Ralf,

    Are you using the correct adapter? The original pinout of XDS110ISO is custom so it wont fit onto typical XDS110 pinout without an adapter

    Regards,

    Peter

  • Hi Peter,

    yes, I have used the included 16pin male to 14 pin female connector. On my pcb I have a 14 pin male connector which works with the XDS110 without isolation.

    Best regards

    Ralf

  • Hi Ralf, 

    Do you have another board that features the 16-pin XDS110 that you can connect to to test the isolated XDS110? Something like controlSOM with controlCARD adapter? 

    Also, what is the JTAG clock speed you are operating at? You may try to reduce the JTAG speed.

    In your layout, which pin is corresponding to 3.3V? One thing you can try is just manually wiring the 4 required signals, TCK, TMS, GND, and 3.3V and then running the XDS test with cJTAG. Forego the adapter in order to verify that the JTAG connection is at least working when the connection is manually verified

    Regards,

    Peter

  • Hi Peter,
    I have solved my problem. The reason was the series resistor R14 on my pcb.

    By using the non isolated XDS110 the pin 5 of the JTAG pin header is only used for detection purposes. Obviously the isolated XDS110 draws a current at this pin which causes a significant voltage drop over this resistor. 
    Now I have removed the resistor and connected the pin 5 direct to 3.3V.

    Best regards

    Ralf