Part Number: TMS320LF2407A
Hi,
we are using a TMS320LF2407A DSP in our product. NOW, after 25 years, we need to make changes in the software for that product.
I am aware that this DSP is old but we still buy it and we still sell those products.
What are my options to maintain that code base? - While reading the forum, I figured out that CCS 3.3 could be a solution, if used on Windows XP but CCS 3.3 is not available for download.
It would be nice, if you could provide a download link to CSS 3.3 so I can try to setup the toolchain.
Any ideas are welcome.
btw.: Our legacy toolchain did not use CCS. We generated the DSP.cmd file and used the compiler, linker, etc directly. - I was able to recover those toolchain files and to migrate them into a modern cmake build. However, the generated out-file is not verified yet. If there are any experiences on this one or if you would like to participate in building an alternative, you are also welcome.
Thanks.