Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1114: SIL2/3 Certified controllers

Part Number: TMS570LS1114
Other Parts Discussed in Thread: HALCOGEN, C2000WARE

Hi,

We are planning to use SIL2/3 certified controllers in one of our design. Below are few queries from my end which i request your support


1. From details from internet, i came to know that TMS570LS12x/11x, RM46x, F28P65x, F280015x,  are the only series which supports SIL2 ? Is that correct? Is there any other series TI recommends?
2. TI provides Safety SW packages to achieve SIL2 & SIL3. Is that correct?
3. Which series of controllers TI recommends to use along with Safety SW to achieve SIL2 or 3?
4. Is the safety SW packages are open source (Free to use) or need to be paid?
5. If any series TI recommends to use; i need evaluation boards and links where i can order from

Request your response for above queries at the earliest.

Thanks
Arfaj S

  • Any update on above queries

  • Hi Syed,

    Apologies for the delayed response, this issue is assigned very recently to me. I want to loop marketing team here to help you to choose right controller for your requirements.

    --
    Thanks & regards,
    Jagadish.

  • Hi Syed,

    1. From details from internet, i came to know that TMS570LS12x/11x, RM46x, F28P65x, F280015x,  are the only series which supports SIL2 ? Is that correct? Is there any other series TI recommends?

    TI offers a broader portfolio of functional safety-compliant microcontrollers:

    1. Hercules Series (Arm-based): TMS570LSx, TMS570LCx and RMx families

    2. C2000 Series (Real-Time Control): TMS320F2838x, F28P65x, F29H85x series 

    3. Sitara AM2x Series: AM243x and AM263x MCU series

    2. TI provides Safety SW packages to achieve SIL2 & SIL3. Is that correct?

    Yes, it is correct. TI provides dedicated software packages to fulfill the diagnostic coverage required by the safety standards.

    1. Hercules SDL and HalCoGen driver, and MCAL driver

    2. C2000Ware STL or SDL 

    4. F29x MCAL driver and SDK/SDL

    3. Which series of controllers TI recommends to use along with Safety SW to achieve SIL2 or 3?

    It depends on your application and system requirements.

    4. Is the safety SW packages are open source (Free to use) or need to be paid?

    The diagnostic software libraries (like the Hercules HalCogen, SDL, MCAL, C2xware STL, etc ), HALCoGen, and the Compiler Qualification Kits are completely free of charge and require no royalties when used with TI hardware. 

    5. If any series TI recommends to use; i need evaluation boards and links where i can order from

    You can evaluate these platforms using the TI LaunchPads or controlCARDs available on the Texas Instruments Store. Please logon TI product pages and find the board you like to use, for example:

    LAUNCHXL2-RM46 Development kit | TI.com