I am working with the Dual Motor Control and PFC Kit and I need a quadrature encoder with 3 channels (A, B and I) to create the speed loop with a sensor. What quadrature encoder recommend me? The file MultiAxis HW Guide does not specify an encoder and I do not know what is best for the motor (Anaheim Automation BLY172S-4000, shaft diameter 5 mm). I would like to work with speeds around 1000 rpm.
In addition, to work with the motor and encoder, will I need Anaheim Automation coupler CPL-HC075-5mm-5mm?
Finally, I have seen in many encoder datasheets that the third channel is called Z or N. Is this the channel I?
Thanks in advance,
Carlos Camacho
Barcelona University