Part Number: F29H850DM
Hi Experts,
I am looking at the Flash Subsystem Block Diagram in the F29 TRM.
Therer is one description:
FRI-1: CPU1 Program FRI-1 interfaces with the instruction fetch bus of the first C29x CPU (CPU1), and is primarily used for executing program code on CPU1. Additionally, FRI-1 is connected to all data read initiators in the system. This read interface has four read ports, numbered RP0 to RP3. These read ports are mapped to code banks depending on the configuration of BANKMODE and BANKMAP.CPU1SWAP registers in the SSU. These settings are described in subsequent sections.
Which saids that the read port is mapped to actual banks depending of banmode. Does this mean that the bank swap is achieved and the read port level, by simply disalbing some of the read ports? is there a table showing which RP is enalbed under specific bankmode and swap status?
In the Figure 8-1, the BANKMODE register goes in to the "Flash Bank Access Router", which means that the router is controlling the access. Can I say that, when CPUx tries to fetch, the fetch request would occurs on all RPs, but the router would decide which RP is actually active, and feed the data on that RP?
Regards,
Hang