Part Number: TMS320F28335
Hello,
I have a question regarding setting up the SYSCLKOUT to 150 MHz on the TMS320F28335.
In our past designs, we used a 25 MHz external oscillator and utilized the setup from to achieve 150 MHz. We configured DSP28_PLLCR as 6 and DSP28_DIVSEL as 3.
However, we recently realized that using DIVSEL = 3 (divide by 1) while the PLL is active is explicitly not recommended according to the Technical Reference Manual.
My question is: what are the potential hardware consequences of running the device with this configuration? We are currently running our devices with this setup without any apparent issues, but could this cause random problems, jitter, or instabilities in the field over time? Like different temperatures?
Thank you