This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000-CGT: C2000 6.2.11 toolchain windows vs linux version

Part Number: C2000-CGT

Hi !

We have to migrate our buildserver for a mature design from windows to linux.

We still use 6.2.11 toolchain on windows and discovered that linux tools with the same version number produces slightly different binaries.

Are there any known issues or recommendations if this is flawless - or is it recommended to stay with the original compiler - and use it in an emulation to get identical binaries - as there might be artefacts ?

rgds.

 

  • Wolfgang,

    The output binary should be identical for the code generation.  Are the differences with diassembled generated code or some non code sections?

    Could you please provide a cut down test case that reproduces the issue?

    Regards,
    Greg