I cannot see the PWM pulses with an oscilloscope when I run "epwm_deadband" or "epwm_updown".
I am using a recent version of controlSUITE and CCS version 5.1.0.09000. I am using the controlCARD TMDXCNCDH52C1 with the XDS100v2 emulator. I am able to load, flash run and debug both programs.
I am probing a pin that has continuity to Concerto pin 5 and comparing it to ground -- in this case I am using pin 3 of J6 on the controlCARD for ground. I am expecting to see a 3.1 volt square wave, but only see low voltage noise. In addition to PA0, I have probed PA1, PA2, PA3, PA4, and PA5 while the programs are running and I see nothing on any of them.
The board and the example programs are original and unmodified.
Is there a switch setting that could make a difference? Does this work for any one else?