Part Number: F29H850TU
Hello TI experts,
On a TMS320F29H850TU9 (REVID at 0x30180028 = 0x1, silicon revision A) that was configured for flash bank mode 2 in HS-FS, the bank mode presents as mode 0 throughout the HS-KP state.BANKMODE at 0x3008005C reads 0x00000009 (BM2) in HS-FS but 0x00000003 (BM0) once the part is in HS-KP, and the BANKMGMT records at 0x10D80000 / 0x10D84000 read back 0x00000000 (access denied) in HS-KP.
Our objective is to provision from HS-KP to HS-SE in a single session, programming the security configuration and the application (including CPU3 / FLC2) without an intermediate reset.
Can you confirm the bank-mode behavior above, and advise how to have bank mode 2 available in KP so that a security configuration, CPU1 and CPU3 content can be programmed in that single session?
Also, while in HS-KP, is it possible to determine the bank mode the device was in before it transitioned into HS-KP, and thus the mode it will be in once it transitions out?
Thank you,
Beat