This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM13E23019: Edge AI Compiler module alone for better delivery

Part Number: AM13E23019

Hi Experts,

Currently the Edge AI compiler comes with the tensorlab repository. However, the repository is big and rely on github conncetion to install. 

The China area has poor github access, which would cause issue when customer try to install it. The down zip option would not work because there are the installation would require git clone in substeps.

For Customer who installs the tensorlab, they are likely to go for BYOM. In this case they can use the compiler only, compiling the artifact from onnx, instead of the whole tensorlab.

Is it compiler in the tensorlab repo can work in standalone? Such that they can download the compiler alone, which should be much easier.

Regards,

Hang