This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: CLB does not output

Part Number: TMS320F280049
Other Parts Discussed in Thread: SYSCONFIG

Dear members,

I was wondering if you can help me: I´m new in FW design using the CLB and I´m experiencing some issues that I cannot make it work... 

Below you can find the code: I want to compare with an AND gate the up_down direction and the PWM CMPC which is set 50%. 

I also tried to just give to the AND gate the "CLB_GLOBAL_IN_MUX_EPWM2_CTRDIR" on all 4 inputs but I do not get any response on the output... 

Any ideas what could be the issue?

Thanks for your support!

#define CFG_OUTLUT_LUT          0x550007
#define LUT4_IN0                        0x18
#define LUT4_IN1                        0x18
#define LUT4_IN2                        0x19
#define LUT4_IN3                        0x19
#define LUT4_FN10                     ((0x00000) | 0xa0a0)
#define LUT4_FN2                       0x0

void ZVS_CLB_Init(void)
{
    EALLOW;
    //Mask Output Channels 4 & 5 (Bits 4 and 5 = 0x30)
    CLB_setOutputMask(CLB1_BASE, (1UL << 4UL) | (1UL << 5UL), true);

    // 1. Enable Peripheral Clocks
    SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLB1);

    ////Initialization of inputs

    // Map IN1 to EPWM2C (Action Qualifier pulse generated at CMPC down-count)
    CLB_configLocalInputMux(CLB1_BASE, CLB_IN0, CLB_LOCAL_IN_MUX_GLOBAL_IN);
    CLB_configGlobalInputMux(CLB1_BASE, CLB_IN0, CLB_GLOBAL_IN_MUX_EPWM2_CTR_CMPC);
    CLB_configGPInputMux(CLB1_BASE, CLB_IN0, CLB_GP_IN_MUX_EXTERNAL);
    CLB_enableSynchronization(CLB1_BASE, CLB_IN0);
    CLB_selectInputFilter(CLB1_BASE, CLB_IN0, CLB_FILTER_NONE);

    // Map IN2 to EPWM1 Counter Direction (1 = DOWN, 0 = UP)
    CLB_configLocalInputMux(CLB1_BASE, CLB_IN1, CLB_LOCAL_IN_MUX_GLOBAL_IN);
    CLB_configGlobalInputMux(CLB1_BASE, CLB_IN1, CLB_GLOBAL_IN_MUX_EPWM2_CTRDIR);
    CLB_configGPInputMux(CLB1_BASE, CLB_IN1, CLB_GP_IN_MUX_EXTERNAL);
    CLB_enableSynchronization(CLB1_BASE, CLB_IN1);
    CLB_selectInputFilter(CLB1_BASE, CLB_IN1, CLB_FILTER_NONE);

    //// Initialization of the output LUT0
    CLB_configOutputLUT(CLB1_BASE, CLB_OUT5, CFG_OUTLUT_LUT);
   
    // Output to a GPIO through the XBAR
    XBAR_setOutputMuxConfig(XBAR_OUTPUT3, XBAR_OUT_MUX03_CLB1_OUT5);
    XBAR_enableOutputMux(XBAR_OUTPUT3, XBAR_MUX03);
    GPIO_setDirectionMode(14U, GPIO_DIR_MODE_OUT);
    GPIO_setQualificationMode(14U, GPIO_QUAL_ASYNC);
    GPIO_setPinConfig(GPIO_14_OUTPUTXBAR3);

    //// Configuration of look up table 0
    // inputs
    CLB_selectLUT4Inputs(CLB1_BASE,LUT4_IN0, LUT4_IN1, LUT4_IN2, LUT4_IN3);
    // function of LUT
    CLB_configLUT4Function(CLB1_BASE, LUT4_FN10, LUT4_FN2);

    EDIS;
    // Enable CLB Tile 1
    CLB_enableCLB(CLB1_BASE);
  • Hi, 

    Please allow me some time to look at your code. I will get back to you in a few days. 

    Kind regards,
    AJ Favela 

  • Dear Aj, 

    I have tried to output the input through the output LUT and even like this i was not able... 

        CLB_configOutputLUT(CLB1_BASE, CLB_OUT5, 0x550018);


    If I try the examples from the CLB they work, but when integrating it in my project, I cannot make it work... Could it be some configuration that I´m missing... 
    Thanks for your support!

  • Hi, 

    Looking at your code the configuration code for the CLB regarding the inputs, outputs, and other configurations looks correct to me. Could you attempt to call initTILE1(); before you call your own custom configuration? 

    Just to confirm, are you attempting to create this with or without the use of syscfg, as our examples within the SDK use syscfg. With syscfg you can use the simulation tool for the CLB to ensure your output is configured correctly. For more information on this please see our appnote. 

    Can you also confirm that EPWM2 is running as expected. Do note that the comments within the code state that both EPWM 1 and 2 are expected to be used, but only EPWM2 is configured as an input. 


    Kind regards,

    AJ Favela 

  • Hi, 

    I used the example code from TI with the sysconfig tool to generate the #define with the 0xYY values.

    Then, I take those defines and I use the functions as in the example  to create my own initTILE() which I name it as ZVS_CLB_Init()

    The PWM2 is working correctly because i´m able to output the PWM A & B.

    It feels as either the CLB is not enable or the output is not written correctly...

    Could it be that i forgot something regarding that? Any compiler settings, something?

    As you did not find anything in the previous code, i will try to work on the example and modify it according to my needs; let´s see if it works. And then move it to my own project.

  • Hi, 

    I was able to run the code in the Launchpad. 

    I found the issue, the HW is populated with the 49 version instead of using the 49C; so no CLB is available. But the good news is that it works good in the Launchpad Slight smile