This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2812 SCI PROBLEM

Hi, I am having some problem wit sci communication. I have the following problem, i am sending values by sci, in a loop. And the first bytes are dummy values (incorrect  information) but then it is working well.

I dont know why the first bytes are incorrect.

I really apreciate your help.

All of configuration registers are correctly configured.

 	SciaRegs.SCICCR.all =0x0007;   
SciaRegs.SCICTL1.all =0x0003;
SciaRegs.SCICTL2.all =0x0000;
SciaRegs.SCIHBAUD =0x0000;
SciaRegs.SCILBAUD =0x0003;
SciaRegs.SCICCR.bit.LOOPBKENA =0; // Enable loop back
SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
 SciaRegs.SCIFFTX.all=0xE040;
SciaRegs.SCIFFRX.all=0x204f;
SciaRegs.SCIFFCT.all=0x0;
I am not using interrupts

This is my code

void average(void)
{
Uint16 fila=0,i=0;

for(i=0;i<9;i++)
{

resultado=mat_datos[0][i];
scia_xmit();
}

}

void scia_xmit()
{
for(ind=2;ind>=0;ind--)
{

sendchar=((resultado >> (ind*8)) & 0x000000FF);
SciaRegs.SCITXBUF=sendchar;
while(SciaRegs.SCIFFTX.bit.TXFFST > 0 ){}

}

resultado=0;
}