Other Parts Discussed in Thread: TMS320F28335
hello,
we were successfully using the tms320f28335 controlcard for motor control applications.
but for the past few days we are encountering the following error:
Error connecting to the target:
Error 0x00001200/-1145
Error during: OCS, Target,
Unrecoverable emulation error
Sequence ID: 0
Error Code: -1145
Error Class: 0x00001200
I/O Port = 0
Board Name: F28335 XDS100 USB Emulator
Cpu Name: TMS320C2800_0
we use code composer studio v3.3 for matlab embedded target support.
i also tried to connect to target via ccsv 4.2 and met with the same error.
on retrying,i was asked to reset the emulator.i tried to do it through
debug option via ccsv3 but no avail.
kindly suggest a way to rectify the problem.our work is halted because of this hangup.
thank you.